Can I configure the NET5301T, NET5301T-I, and SP04-140 using a web browser?

Issue

Can I configure the NET5301T, NET5301T-I, and SP04-140 using a web browser?

Product Line

Pelco Video Management

Environment

Endura NET5301T/NET5301T-I/SP04-140- All versions

Cause

Need to know if the encoders can be configured through a web interface.

Resolution

There is no web browser option. Menu options are available using the WS5000 Advanced System Management Software.