How do I connect to the SM5000 System Manager web configuration menu?

Issue

How do I connect to the SM5000 System Manager web configuration menu?

Product Line

Pelco Video Management

Environment

  • SM5000

Cause

The SM5000 web interface is used for various purposes, amongst which DHCP and NTP and is a crucial part of the initial set-up of an Endura system.

Resolution

Use the following procedure to access the configuration menu.

  1. Open a web browser.
  2. In the address bar type https://[SM5000 IP address]:10000. For example, https://192.168.5.10:10000.
  3. Select the browsers go option or press enter. If presented with a security warning it will be necessary to accept this message before preceding. 
  4. When prompted, enter the username and password. The default username is admin and the default password is admin.
  5. Click the Login button.