When adding Sarix cameras to an Endura 1.0 system, what Endura 2.0 devices will I need to view and record video?

Issue

When adding Sarix cameras to an Endura 1.0 system, what Endura 2.0 devices will I need to view and record video?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Endura 1.0 system
  • Sarix H.264 cameras- All versions
  • NET5500 Series Encoders - All Versions

Cause

Information on the compatibility of Sarix cameras with the Endura 1.0 system is needed.

Resolution

If a high definition H.264 Sarix camera is to be used with an existing Endura 1.x system the following will be needed;

  • NSM5200 for H.264 recording.
  • One or more of the following for viewing of live or recorded H.264 video; WS5200, VCD5202, or NET5402R-HD.

Endura 1.x systems can natively support all standard definition MPEG-4 Sarix cameras (IXS0,IES0,IDS0, and IMS0). If a standard definition MPEG-4 Sarix camera is used then there are no additional devices needed.