Can I run video, control the IP Spectra IV on a monitor and also view it over the Internet at the same time?

Issue

Can I run video, control the IP Spectra IV on a monitor and also view it over the Internet at the same time?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP
  • Spectra IV IP H.264

Cause

Simultaneous IP and Analog video option

Resolution

Yes, the older versions needed to be connected to the internet or you could not control them. Currently you can control them with a D protocol if wired as such and view the video, concurrently with internet viewing.