How do I connect to an IP camera?

Issue

How do I connect to an IP camera?

Product Line

Pelco Cameras

Environment

  • Sarix
  • Spectra HD
  • SD4N23-PG-E0 (IP Spectra IV)
  • SD4E Series
  • Esprit IP
  • Spectra Mini IP
  • IP110
  • IP3701

Cause

Incorrect login credentials or IP range.

Resolution

To access the IP camera do the following:

  1. Open the Web browser.
  2. Enter the IP address of the IP camera in the browser's address bar. The Login screen opens. 
  3. Enter admin (all lowercase) in the User ID and Password fields (admin is the default setting for these fields).
  4. Click Login In.