Does the CM9700 Matrix System support network connection to the Spectra IV IP?

Issue

Does the CM9700 Matrix System support network connection to the Spectra IV IP?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM9700 Matrix
  • Spectra IV IP

Cause

Spectra IV IP connection

Resolution

The Spectra IV IP dome systems allow you to control and monitor video over an IP network. The CM9700 systems do not support the Spectra IV IP network connection.