Does Spectra IV IP Series support 255 presets?

Issue

Does Spectra IV IP Series support 255 presets?

Product Line

Pelco Cameras

Environment

  • DD423
  • DD427
  • DD429
  • DD436

Cause

Amount of supported presets

Resolution

The Spectra IV SL dome system, which includes 23X models, has 64 preset positions. The presets that can be configured are numbered 1 to 32 and 35 to 64.

The Spectra IV SE dome system, which includes 27X and 35X models, has 256 preset positions. The presets that can be configured are numbered 1 to 32, 35 to 82, and 100 to 255.