What is the difference between the Endura NET5308T and NET5308T-EXP video encoders?

Issue

What is the difference between the Endura NET5308T and NET5308T-EXP video encoders?

Product Line

Pelco Video Management

Environment

  • Endura NET5308T- All versions
  • Endura NET5308T-EXP- All versions

Cause

Information regarding the differences between the NET5308T and the NET5308T-EXP model numbers is needed.

Resolution

The part number NET5308T includes one NET5300B base unit video server and one NET5308T-EXP expandable video input unit. Purchasing the NET5308T part number will provide up to 8 video inputs. To get 16 video inputs, purchase one additional NET5308T-EXP. The base unit will support up to a maximum of 16 video inputs.