How to access a Sarix camera's built-in web application

Issue

How do users access a Sarix camera's built-in web application?

Product Line

Pelco Cameras

Environment

  • Sarix
  • Internet Explorer 7 or later
  • Mozilla Firefox 3.0 or later
  • Apple Quicktime

Cause

NoteThe following are minimum requirements for accessing the Sarix web application:

  • Microsoft Internet Explorer 7 (or later)
  • Mozilla Firefox 3.0 (or later)
  • Quicktime

NoteThe latest versions of Quicktime (certain version of 7.x and 10.0 for Mac OSX or 7.64 for Windows) contains a bug that prevents it from playing RTSP streams.

Resolution

To access a Sarix camera's web application:

  1. Type the camera's network location (IP address) into a compatible web browser.
  2. Once you access the web application, click on the login link on the top right in order to access the web application's other features such as configuration.
  3. When the login screen appears, use the default username and password values (username:admin / password:admin).

For more information regarding a Sarix camera's web application, please refer to IX Series Network Camera documentation C2950M-A. This can be found within Sarix camera product pages at http://pelco.com.