RTSP Server allows the viewing and control of both live and playback streams using a standard RTSP client.

Issue

RTSP Server allows the viewing and control of both live and playback streams using a standard RTSP client.

Product Line

Pelco Video Management

Environment

RTSP server- All versions

Cause

Information regarding the RTSP server is needed.

Resolution

Overview

The RTSP Server allows the viewing and control of both live and playback streams using a standard RTSP client (e.g. VLC, Quicktime, or a custom built client such as Pelco's PelcoAPIViewer). The RTSP Server can be used to view both live and playback video. It could also be used to obtain an SDP description for the older Endura cameras and encoders.

For additional details reference the RTSP Server document.