Can I access the Sarix stream from any computer via a RTSP URL? If so, what is the format of the URL Pelco uses? What is the Web Url RTSP Stream

Issue

Can I access the Sarix stream from any computer via a RTSP URL? If so, what is the format of the URL Pelco uses?

Product Line

Pelco Cameras

Environment

  • SARIX
  • RTSP Stream
  • What is the Web Url RTSP Stream

Cause

View of RTSP URL stream.

Resolution

These video streams cannot be opened in a normal web browser without a video player of some kind. however, a single JPEG image be viewed in your web browser. To view a single motionless image: can visit http://[IP address of the camera]/jpeg

Use VLC Player to access these streams.

Unicast Streams:
RTSP URL stream 1:  rtsp://<ip_address camera>/stream1
RTSP URL stream 2: rtsp://<ip_address camera>/stream2

Multicast Streams:
RTSP URL stream 1:  rtsp://<ip_address camera>/stream1m
RTSP URL stream 2:  rtsp://<ip_address camera>/stream2m

Example: rtsp://192.168.0.20/stream1

 

Related Topics:

What is the URL (HTTP,RTSP) for a live stream from a Sarix camera or encoder?