What is the Remove NVR Associations feature in Endura Utilities and when should I use it?

Issue

What is the "Remove NVR Associations" feature in Endura Utilities and when should I use it?

Product Line

Pelco Video Management

Environment

Endura Utilities- All versions

Cause

Cameras are associated to an old recorder and are not available to be added to a new recorder.

Resolution

The "Remove NVR Associations" feature in Endura Utilities is used to un-associate a camera from a recorder.  This should be used if that particular camera will need to be recorded to a different NSM5200 recorder.