The EH8000RKIT new model's refill head will not fit into the Spectra IV pressurized lower dome.

Issue

The EH8000RKIT new model's refill head will not fit into the Spectra IV pressurized lower dome.

Product Line

Pelco Cameras

Environment

  • EH8000RKIT
  • Spectra IV pressurized

Cause

The EH8000RKIT now has a larger refill head than the previous style head which is no longer available. The new model's head will not fit into the Spectra IV pressurized lower dome.

Resolution

An adapter is available to allow the refill head to fit the Spectra IV pressurized lower dome. The part is a non-Pelco part and is made by Camel, the part number is 38-314-50. An extension similar to the Camel extension can be found at almost any auto parts retailer. The extension is used for a tire pressure valve. The Spectra IV pressurized lower dome is in the process of being reworked to compensate for the new larger refill head. The old EH8000RKIT's will need the adapter.