Is the FS85011 series fiber card compatible with the Spectra IV HD?

Issue

Is the FS85011 series fiber card compatible with the Spectra IV HD?

Product Line

Pelco Cameras

Environment

  • FS85011 Series fiber card
  • Spectra IV HD

Cause

The Spectra IV HD does not provide a plug in terminal block similar to the standard spectra series cameras.

Resolution

No. The Spectra IV HD will require external ethernet fiber product.

Refer to Pelco Fiber Optics page for fiber information and model number.