How can I access my IP110 camera from home?

Issue

How can I access my IP110 camera from home?

Product Line

Pelco Cameras

Environment

  • IP110 Models

Cause

Remote viewing of IP110

Resolution

In order to access the IP110 from home you must have the IP address of the site where it is located. You also must have the proper ports opened to get through any firewalls. These ports are 80, 25, 8080, 49152, 49156, 9000-9200, and 443.  The IP110 uses port 80 and cannot use port forwarding or name address translation. You then use the direct IP address of the camera to view it