What are the key differences between the DX8100 software version 1.0 and 2.0?

Issue

What are the key differences between the DX8100 software version 1.0 and 2.0?

Product Line

Pelco Video Management

Environment

  • DX8100 series version 1.0
  • DX8100 series version 2.0

Cause

Compare DX8100 version 1.0 to 2.0

Resolution

The below features are supported with v2.0.
• Supports Pelco and AXIS Standard Definition IP Cameras
• DIACAP-Compliant
• USB 2.0 JBOD External Storage Supports up to 8 TB
• Internal Storage Capacity up to 8 TB