What is the CM9760-CDU-T Code Distribution Unit?

Issue

What is the CM9760-CDU-T Code Distribution Unit?

Product Line

Pelco Matrix

Environment

CM9760-CDU-T

Cause

Product Specification

Resolution

The CM9760-CDU-T code distribution unit is a 16-channel RS-422 transmit-only (two data wires and ground) data distribution unit. It can be used with any system that uses RS-422 serial communications. The CDU is used to install pan/tilt and dome receivers in a “star,” or “home run,” configuration.