Is the CM9760-CXTA Coaxitron Translator compatible with third-party DVR?

Issue

Is the CM9760-CXTA Coaxitron Translator compatible with third-party DVR?

Product Line

Pelco Transmission & Power

Environment

CM9760-CXTA

Cause

Coaxitron® protocol for command and control functions.

Resolution

Yes, as long as the DVR supports Pelco RS422 Pelco P or D protocol.

Note: Review your DVR programming and physical connection options when considering use of Pelco Product for integration.

  • Does DVR require RS232-RS422 convertor for connection?
  • Verify programming options of P or D protocol and its associated Baud Rate setting: (2400, 4800,9600)