Issue
What is the bandwidth requirement for each Spectra IV IP?
Product Line
Pelco Cameras
Environment
Spectra IV IP
Cause
Bandwidth usage
Resolution
The bandwidth for the Spectra IV-IP Atlas based module is 3 Mbps for both MPEG4 using 30 IPS (images per second) and 3 Mbps for MJPEG when using 15 IPS (maximum allowed for this module). The bandwidth for the newer Sarix based Spectra TXB-N module is 2 Mbps for both H.264 and MPEG4 when set to 30 IPS . This module uses as much as 5.4 Mbps in MJPEG mode if set for 30 IPS.