What are the available formats for exporting video from a Digital Sentry system?

Issue

What are the available formats for exporting video from a Digital Sentry system?

Product Line

Pelco Video Management

Environment

  • Digital Sentry
  • DSSRV
  • DSNVS
  • DS Control Point software

Cause

Some formats required additional software

Resolution

The available video formats are:

  • AVI (Indeo) (does not work removed in later version).
  • AVI (Video 1) (playable in windows media player or VLC Media player, but can export only one camera at a time)
  • EXE (a self-extracting executable with in DS Media Player built in)
  • H264 (playable in VLC Media player)
  • MJPEG (playable in windows media player or VLC Media player)
  • MPEG1 (playable in windows media player or VLC Media player)
  • MPEG2 (playable in windows media player or VLC Media player)
  • MPEG4 (playable in windows media player or VLC Media player)
  • XPA (playable in DS Media player)

Note: EXE, XPA capability

  • Will include audio. (if available on digital sentry)
  • Authenticate Video option (To verify that the video displayed has not been corrupted)
  • Multiple camera video export.