What is the IR nanometer range of Spectra IV?

Issue

What is the IR nanometer range of Spectra IV?

Product Line

Pelco Cameras

Environment

  • DD427
  • DD435
  • DD436

Cause

IR wavelength range of Spectra

Resolution

When using an IR illuminator, the "Low Light Focus" feature of the camera can be tuned to correspond to the setting of the illuminator. There are three low light focus settings:

  •  OFF (default): Low light focus is not activated.
  • 850NM: Low light focus is tuned to 850 nm (nanometers).
  • 950NM: Low light focus is tuned to 950 nm.