Can I manually assigned a static IP address to a Spectra IV IP?

Issue

Can I manually assign a static IP address to a Spectra IV IP?

Product Line

Pelco Cameras

Environment

  • SD4N Models
  • SD4E Models

Cause

Programming of Static IP

Resolution

Yes. A static IP address may be assigned to the Spectra IV IP.

Administrator Log In is required to the web interface.

  • View LL#8800 for connection to a network