DS ControlPoint version 7.0.8, users now have the ability to export video directly to a CD/DVD.

Issue

Cannot export video directly to a CD/DVD from DS ControlPoint.

Product Line

Pelco Video Management

Environment

  • DS ControlPoint v7.0.8
  • Microsoft Windows XP

Cause

Required applications are not installed to allow ControlPoint to export to CD/DVD.

Resolution

When utilizing DS ControlPoint version 7.0.8, users now have the ability to export video directly to a CD/DVD.

Two applications are required for this option to function:

The user will be prompted to restart their computer after installing the applications.