Can the Endura NVR5100 and NSM5200 reside in the same network or VLAN?

Issue

Can the Endura NVR5100 and NSM5200 reside in the same network or VLAN?

Product Line

Pelco Video Management

Environment

  • Endura NVR5100- All versions
  • Endura NSM5200- All versions

Cause

Information regarding the functionality of an NVR and NSM on the same network is needed.

Resolution

For design purposes and consideration, the NSM5200 needs to reside in its own VLAN.  The NVR5100 by design will record any cameras introduced to its VLAN.