Does Sarix support Daylight Savings Time (DST)?

Issue

Does Sarix support Daylight Savings Time (DST)?

Product Line

Pelco Cameras

Environment

Sarix cameras- All versions

Cause

Information regarding the availability of DST on Sarix cameras is needed.

Resolution

The Sarix cameras do not hold local time. Instead, they rely on an external NTP server to provide the time for it.
If the external NTP server supports DST, that will push down to the camera.