Can I view video over coax and use the IP video at the same time on the Spectra IV IP ?

Issue

Can I view video over coax and use the IP video at the same time on the Spectra IV IP ?

Product Line

Pelco Cameras

Environment

  • SD4N Models

Cause

Product Feature of Spectra IV IP for simultaneous IP and Analog Video and Control

Resolution

Yes. The Spectra IV IP can send video and encode video at the same time. If controlled from a head end controller and internet controller, usually the head end controller will over ride the internet controller when commands are sent out such as pan and tilt.