Is NTCIP an internet protocol that connects to the web from the TXB board?

Issue

Is NTCIP an internet protocol that connects to the web from the TXB board?

Product Line

Pelco Transmission & Power

Environment

TXB-NTCIP translator board

Cause

Verify if the TXB-NTCIP board support internet protocol.

Resolution

No.  When using a TXB-NTCIP, the output is still analog. NTCIP stands for National Transportation Communications for ITS Protocol. ITS stands for Intelligent Transportation system. This is a protocol to standardize the transportation communication systems. It can go over the internet but is not necessarily internet only based.