How do I reset the Spectra IV IP H264 to factory defaults using a Web Browser?

Issue

How do I reset the Spectra IV IP H264 to factory defaults?

Product Line

Pelco Cameras

Environment

Spectra IV IP H.264

Cause

Reset stored settings

Resolution

To reset the Spectra IV IP H.264 from software,

  1. Log into the camera from the web page.
  2. Go into the "system" heading from the "settings" section on the top right.
  3. Click on reset the camera to factory defaults. The camera will reboot.

The process takes about 8 minutes to complete. There is no hardware reset button.