If the DS NVS connects to a 4 channel Axis Server, how do I know which channel is which?

Issue

If the DS NVS connects to a 4 channel Axis Server, how do I know which channel is which?

Product Line

Pelco Video Management

Environment

  • Digital Sentry
    • All DS hardware
  • DS NVs
  • AXIS server encoder

Cause

New Digital Sentry install with a AXIS server encoder.  

Resolution

When connected to an Axis Server (encoder), each channel will be given its own IP Address as well as license. At that point, each channel can be renamed based on the installation.