How can I restore a backup in DS NVS?

Issue

How can I restore a backup in DS NVS?

Product Line

Pelco Video Management

Environment

DS NVS

Cause

Corrupt database on the system require a database rebuild to sync the database with the actual video storage on the system.  

Resolution

To restore a back up from DS BackUP on an NVS system, follow the below instructions:

1. Open the DS Backup Manager application

2. Under the Restore area, click the Restore Archived Settings

3. Once completed, the Current Status will state Completed