How do I setup DS Admin in Digital Sentry NVR?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do I setup DS Admin in Digital Sentry NVR

Product Line

Pelco Video Management

Environment

DS NVR (all version)

Cause

Configures DS NVR for daily use

Resolution

To setup DS Admin in the NVR system, complete the following steps:

1. To run the DSAdmin program, select it from the Start menu

2. Enter your logon information

When DSAdmin first runs, the name of the client computer appears in the gray title bar and the Folder Items area. The Server List field contains a path to a local .INI file containing a list of servers to which it can be connected by the client.

NOTE: If the logon information entered during DSAdmin startup does not match the logon information for the available systems, you are also asked to enter logon information for those system.