How do I add a new keyboard to the CM9700 Series Matrix System?

Issue

How do I add a new keyboard to the CM9700 Series Matrix System?

Product Line

Pelco Matrix

Environment

  • CM9700 Matrix
  • CM9700 System Manager

Cause

Adding CM9760-KBD

Resolution

All devices for the CM9700 matrix are added with the add device wizard in the System Manager software. 

  1. Run the CM9700 Manager Program and Log in.
  2. Click on the add device wizard and select the keyboard you are adding, then follow the wizard.