Is the Endura UDI5000-CAM Universal Device Interface compatible with the DVR5100 series hybrid video recorder?

Issue

Is the Endura UDI5000-CAM Universal Device Interface compatible with the DVR5100 series hybrid video recorder?

Product Line

Pelco Video Management

Environment

  • Endura UDI5000-CAM- All versions
  • Endura DVR5100- All versions

Cause

Information on the compatibility of the UDI5000-CAM with the DVR5100 is needed.

Resolution

No. The UDI5000-CAM is not compatible with DVR5100 series and Endura 1.0 network video recorders such as the DVR5300 and NVR5100 series.

The UDI5000-CAM is compatible only with the Endura 2.0 network video recorders such as the NSM5200 and EnduraXpress EE500 series.