Will the Endura SM5000/SM5200 Manager DHCP service support network IP Address classes A, B, and C?

Issue

Will the Endura SM5000/SM5200 Manager DHCP service support network IP Address classes A, B, and C?

Product Line

Pelco Video Management

Environment

Endura SM5000/SM5200 -All versions

 

Cause

Need to configure VLANs for the DHCP server on the SM5000/SM5200.

Resolution

Yes.
 

IP Address Class IP Range Largest CIDR block (subnet mask)
Class A  10.0.0.0 – 10.255.255.255 10.0.0.0/8 (255.0.0.0)
Class B 172.16.0.0 – 172.31.255.255 172.16.0.0/12 (255.240.0.0)
Class C 192.168.0.0 – 192.168.255.255 192.168.0.0/16 (255.255.0.0)