How do I change the field of view on an IP110 series camclosure?

Issue

How do I change the field of view on an IP110 series camclosure?

Product Line

Pelco Cameras

Environment

  • IP110-DN Models
  • IP110-CHV Models

Cause

Need to zoom in or zoom out lens to adjust for scene

Resolution

To adjust the field of view:

 
  1. Loosen the zoom locking screw (refer to figure below).
  2. Turn the zoom adjustment ring clockwise or counterclockwise to select the field of view. 
  3. Tighten the zoom locking screw.