How do I determine the incoming bitrate that the NSM5200 is receiving from the cameras?

Issue

How do I determine the incoming bitrate that the NSM5200 is receiving from the cameras?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Cause

The incoming bit rate is needed.

Resolution

  1. Launch Endura Utilities, log in and press Search.
    note:The default login credentials for Endura Utilities version 2.2 and below is [Username: Administrator and Password: configapp], however version 2.3 and greater removed that unique login credential requirement, and instead authenticates against the standard Endura Credentials. The default login in that case is [Username: admin and Password: admin].
  2. Locate the NSM5200 in question. note: An NSM member will be listed under model name NSD.
  3. Right click on the NSM and choose Open Web Interface.
  4. Login to the web interface, the default password is admin.
  5. The incoming bitrate can be viewed in the System Status tab.