Can multiple NSM5200 storage pools reside in the same network or VLAN?

Issue

Can multiple NSM5200 storage pools reside in the same network or VLAN?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Cause

Information on the placement of NSM pools on the network is needed.

Resolution

Yes. Since the NSM5200 does not automatically record Endura encoders or IP-based cameras, it is possible to configure multiple storage pools in the same network or VLAN.