Minimum system requirements for the Sarix IEE Series.

Issue

What are the minimum system requirements for the Sarix IEE Series?

Product Line

Pelco Cameras

Environment

Sarix IEE Series

Cause

Minimum System Requirements to support the Sarix IEE Series.

Resolution

Minimum System Requirements

  • Processor: Intel Core 2 Duo microprocessor, 2.6 GHz
  • Operating System: Microsoft Windows XP, Windows Vista, or MAC OS X 10.4 (or later)
  • Memory: 2 GB RAM
  • Network Interface Card (NIC): 100 megabits (or greater)
  • Monitor: Minimum of 1024 x 768 resolution, 16- or 32-bit pixel color resolution
  • Web Browser: Internet Explorer 7.0 (or later) or Mozilla Firefox 3.5 (or later); Internet Explorer 8.0 (or later) is recommended for configuring analytics
  • Media Player: QuickTime 7.6.5 for Windows XP, Windows Vista, or QuickTime 7.6.4 for MAC OS X 10.4