How can I control a Spectra camera on a DX8100 HVR (Hybrid Video Recorder) looping through a CM9700?

Issue

How can I control a Spectra camera on a DX8100 HVR (Hybrid Video Recorder) looping through a CM9700?

Product Line

Pelco Cameras, Pelco Video Management, Pelco Matrix

Environment

  • DX8100 Series HVRs
  • CM9700 Matrix
  • Spectra

Cause

Installation of the Spectra series camera so users on the DX8100 recorder can control the camera.

Resolution

To control a Spectra Series camera looping from the CM9700 matrix and DX8100 Series, make sure the Matrix system is first in the looping process. Loop the camera from the Matrix cards to the DX8100 Series. The DX8100 series is the last part of the looping system.