How do I remove a USB device from the DX8000/DX8100 HVR (Hybrid Video Recorder) after exporting video?

Issue

How do I remove a USB device from the DX8000/DX8100 HVR (Hybrid Video Recorder) after exporting video?

Product Line

Pelco Video Management

Environment

  • DX8000 Series recorder
  • DX8100 Series recorder
  • USB device

Cause

Properly remove attached USB device from the recorder

Resolution

REMOVING A USB FLASH DRIVE

You can remove a USB device within the DX8100 environment. In this case, you do not have to exit to the Windows environment.

WARNING: Improperly removing a USB drive can cause data to be lost or corrupted.

 

To remove the USB flash drive from the DX8100:

1. Click > File Unplug/Eject Hardware. The Unplug or Eject Hardware dialog box opens.

2. Select the USB flash drive in the Hardware devices list.

3. Click Stop. The Stop a Hardware device dialog box opens.

4. Select the USB device.

5. Click OK.

6. Wait for the DX8100 to respond with a message stating that it is safe to remove the USB device from the DX8100. Removing a USB flash

drive before the DX8100 acknowledges that it is safe to do so, might result in lost or corrupted data.

7. Remove the USB flash drive.