How to configure a Park Time Action on a Spectra IV PTZ camera using the DX4500/DX4600/DX4700/DX4800 DVR?

Issue

How to set the Spectra camera to Park Time Action on the DX4500/DX4600/DX4700/DX4800 DVR?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • DX4500/DX4600
  • DX4700/DX4800
  • Spectra Series

Cause

Programming steps to set park action of Spectra.

Resolution

In order to set the camera in park time mode, follow the instructions below:

  1. Select the PTZ camera on the DX4500/4600 server
  2. Open the PTZ command keypad from the tool bar
  3. Click the PGM button
  4. The Spectra Menu will appear on the screen
  5. Scroll down to Dome Settings and click the Iris + button to enter the menus
  6. Scroll down to Motion and click Iris +
  7. Scroll down to Park Time Minutes and change the minutes for your scenario
  8. Scroll down to Part Time Action to change the action for camera
  9. Once the settings are changed, click the Iris - to go directly to Exit
  10. Click Iris + to exit the Spectra Menu