SPECTRA III AND IV TXB PLUG PART NUMBER

Issue

I have removed the plug for the TXB board on a Spectra III/IV, how can I obtain a new one?

Product Line

Pelco Cameras

Environment

Spectra III/IV Series
TXB board

Cause

TXB board is removed from the Spectra dome and required to re-install to avoid any potential connection problems with the exposed connection.

Resolution

The TXB connector plug that is removed when a TXB board or Fiber board is installed into a Spectra back box can now be ordered through sales. The part number is TXB-HEADER.