In the Endura WS5000 Advanced System Management Software, what is the difference between camera groups and location?

Issue

In the Endura WS5000 Advanced System Management Software, what is the difference between camera groups and location?

Product Line

Pelco Video Management

Environment

Endura WS5000- All versions

Cause

Information regarding the difference between location and camera groups within the WS5000 software is needed.

Resolution

Basically, camera groups and location are two ways to organize cameras. Cameras may be organized based on physical location, and within each location, would be different camera groups. If you have a very large system with hundreds of cameras, you may want to rearrange the cameras displayed in the Explorer view based on location, camera groups, camera number, or camera name.