Are the Endura GW5000 Gateway and CM9700MDD-EVS compatible with the EnduraXpress EE500 series network video recorder?

Issue

Are the Endura GW5000 Gateway and CM9700MDD-EVS compatible with the EnduraXpress EE500 series network video recorder?

Product Line

Pelco Video Management

Environment

  • Endura EE500- All versions
  • Endura GW5000- All versions
  • Endura CM9700MDD-EVS- All versions

Cause

Information on the compatibility of the EE500 with the GW5000 and the CM9700MDD-EVS is needed.

Resolution

The EnduraXpress EE500 does not support the Endura GW5000 or the CM9700MDD-EVS.