Pelco Product CAD drawings

Issue

Where can I obtain CAD drawings?

Product Line

Pelco Cameras, Pelco Monitors, Pelco Video Management, Pelco Matrix, Pelco Transmission & Power

Environment

Pelco product diagrams / CAD file

Cause

  • CAD drawings are now associated with a pelco.com page location for Downloads & Documents.
  • Download Pelco products in CAD (Computer-aided design) file formats to assist in design purposes.

Resolution

To obtain product diagrams:
  1. Go to Support area.
  2. Click on the interested product category (Video Management, Camera, Accessories)
  3. Choose a Product Offer
  4. Choose "Technical Drawings" for Asset Type
    NOTE: Product diagrams / CAD files are only available for selected products. If the option "Technical Drawings" is unavailable, then no drawing is available for that product.

 

NOTE:

  • Request of CAD drawings not available via Pelco.com are made through the A&E manager for region. Contact the manager for the specific region and submit the request. 
  • There is also the Architect and Engineer Services Registration. By completing the form customers are provided with a direct contact for all the Pelco A&E needs. The form is filled out and submitted here: Registration Form