When is the Endura NET5301-TC transcoder required?

Issue

When is the Endura NET5301-TC transcoder required?

Product Line

Pelco Transmission & Power

Environment

Endura NET5301-TC- All versions

Cause

Information regarding the usage of the NET5301-TC is needed.

Resolution

The NET5301-TC transcoder converts MPEG-4 video from the Endura ® network into formats that are compatible with public networks with limited bandwidth, such as a local area network (LAN), wide area network (WAN), or the Internet.