How do I access the DVR5100 hybrid video recorder configuration menu?

Issue

How do I access the DVR5100 hybrid video recorder configuration menu?

Product Line

Pelco Video Management

Environment

Endura DVR5100- All versions

Cause

The DVR5100 recorder configuration menu is needed.

Resolution

To access the DVR5100 configuration menu press the M key on the keyboard [or Menu button] to display the Main menu. From the Main menu select Setup using the mouse or the red function button. If you don’t see Setup, press the Backspace key on the keyboard, or click Back using the mouse.