Issue
How do I enable the alarm dongle?
Product Line
Pelco Cameras
Environment
- ALM-1
- Spectra HD
- Sarix Camera Models
Cause
Alarm Connections
Resolution
Once the dongle is installed, it is plug and play. Sometimes you may have to restart the camera after installing it to make sure the camera sees it. After that you should be able to program the alarm inputs and relay outputs.