Can the Exsite IP series explosion proof use RS422/RS485 control connections and an analog Controller such as the KBD300A?

Issue

The Exsite IP series explosion proof is a Sarix based network camera that does not support any analog connections.

Product Line

Pelco Cameras

Environment

Exsite IP series explosion proof - All models

Cause

Sales, Installation, and Maintenance.

Resolution

The Exsite has pinouts on the wire harness that resembles a RS422/485 connection, but this is an ethernet connection.