What is the maximum number of remote clients that can simultaneously playback video from a NSM5200 storage pool?

Issue

What is the maximum number of remote clients that can simultaneously playback video from a NSM5200 storage pool?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Cause

Information on the number of remote clients that can playback video from an NSM pool simultaneously is needed.

Resolution

NSM5200 supports playback of 32 video streams per pool, including video export via WS5000 and VideoXpert.  Therefore, if there is a lot of activity through multiple client PCs reviewing video and exporting video clips, the users need to ensure the 32-stream limitation is not exceeded; there are no warnings or other errors displayed, the playback or export simply fails.